Other Parts Discussed in Thread: IWR1443BOOST, , UNIFLASH, IWR1642, IWR1443
Hi,
I'm having problems running the Labs provided in the TIREx. I'm also using the IWR1443BOOST. I have the mmwave_sdk_03_03_00_03 and the Industrial Toolbox 4.2.1 installed. I am using a 5V, 3A power adapter an the USB cable provided with the IWR1xxx.
IWR1642BOOST:
- I filtered the content of the TIREx so only the content with support for the IWR1642BOOST is shown using the autodetect function.
- I choose the "16xx - High Accuracy Range Measurement" Lab.
- I put the EVM in Flashing Mode as described in the User's Guide of the TIREx
- I started Uniflash and selected the right COM in "Settings & Utilities"
- I flashed the prebuilt binary "xwr16xx_high_accuracy_mss.bin" successfully and exited the Uniflash tool
- I put the EVM in Functional Mode as described in the User's Guide of the TIREx
- I ran the High Accuracy Visualizer from Chrome Browser and setup the COM ports correctly but the connection to the target couldn't be established. It just stays in the "connecting to 1 of 2 targets" state (waiting for data.. on both COM ports)
I'm using the EVM with IWR1642 ES2.0 (Rev. 2) but it is not mentioned that the ES3.0 necessary. So why is the software unable to establish a connection? I have the some problem with the Obastacle Detection Lab of the Automation Toolbox 2.9.1.
IWR1443BOOST:
- I filtered the content of the TIREx so only the content with support for the IWR1443BOOST is shown using the autodetect function.
- I choose the "14xx - High Accuracy Range Measurement" Lab.
- I put the EVM in Flashing Mode
- I started Uniflash and selected the right COM in "Settings & Utilities"
- When I tried to flash the prebuilt binary "xwr14xx_high_accuracy_mss.bin" Uniflash reported folowiing error
[5.4.2020 12:40:41] [INFO] Cortex_R4_0: Header of C:/ti/mmwave_industrial_toolbox_4_2_1/labs/level_sensing/14xx_high_accuracy/prebuilt_binaries/xwr14xx_high_accuracy_mss.bin file indicates it is not a valid file to flash to IWR1443: 0x5254534d[5.4.2020 12:40:41] [ERROR] Cortex_R4_0: !!! Aborting flashing of specified files!!!
I'm using the EVM with IWR1443 ES2.0 (Rev. 2) but it is not mentioned that the ES3.0 necessary. So why is file not valid?
Best regrads
Bruno