This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

follow up to a particular thread.

Intellectual 520 points

Replies: 5

Views: 1443

Hello,

                I would like to know how to follow up to a particular thread if i have same issue as mentioned in the thread.

B.R

Gourav

B.R.

Gourav

  • Hello Gourav,

    If you want to reply to add information that is relevant to a particular thread, use the Reply button. If you have a similar problem use the Ask a related question button in the top right hand of the page from the original thread.

    Thanks
    Bill

    Bill Traynor
    E2E SysAdmin/DevOps

  • In reply to William Traynor:

    Hello Bill,
    Is any option to receive notifications of a particular existing thread??
    B.R.
    Gourav

    B.R.

    Gourav

  • In reply to Gourav H:

    Hi Gourav,

    Yes, on the thread you wish to track, but have not Replied to, click on the Options button at the right-side of the page, then click on the "Reply notifications are off"; this will change the setting to "Reply notifications are on" and you will receive an email each time an additional Reply is posted.

    At your service,

    ~Leonard     

  • I would like to also ask, If I want to do a follow up on a locked thread, is there a way to ask for it to be unlocked?

    Soooo many computers, sooo little time.

  • In reply to Cool Javelin:

    Hi Cool,

      Yes, there is a way for an admin to UNLOCK a thread, but an even easier way for a user to ask another question is to click the    button .

    This will place the link to the locked (or not) thread at the top of the newly-created thread so all can see and reference the originating thread.  Simply click that link, everything else is handled automatically for you.

    Regards,

    ~Leonard

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.