This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

suggestion: save draft when writing

Prodigy 140 points

Replies: 1

Views: 60

Dear ladies/gentlemen,

Today I was busy to respond to a message I got. While typing and uploading several screenshot the browser suddenly crashed and the whole stuff I wrote was gone so I have to type all things once again. This is very annoying. To prevent the user from loosing the text and the time spent on it, I want to ask you if it will be possible that the message someone is writing can be saved as draft each minute? When the user comes back then the draft still available and automatically restored so that the user can go on. This would be very very nice and highly appreciated.

Thanks in advance.

  • Hello

    Thank you for the feedback, we sincerely appreciate it.  We do maintain an enhancement list for consideration and will add your suggestion.  

    Bill Traynor
    E2E SysAdmin/DevOps

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.