This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TS3DV642: Terminal Processing when CEC,CEC-A,CEC-B Pin unused for TS3DV642

Genius 5575 points

Replies: 2

Views: 352

Part Number: TS3DV642

Dear sirs,

My customer asked us about terminal Processing when CEC,CEC-A,CEC-B Pin unused   for TS3DV642.

The customer does not connect these pins to the HDMI terminal or control device.
CEC is connected between HDMI terminals.
Under these conditions, they are asking us how to handle the CEC, CEC-A, CEC-B terminals.
When I checked the data sheet, I think that connecting to VDD or GND from the description below in (6) of 6.3 Recommended Operating Conditions on page 5.

Is this correct?

Best Regards,

Y.Hasebe

  • Hasebe,

    The section of the datasheet you are referring to is meant for the EN, SEL1, SEL2 pins of the TS3DV642. The CEC, CEC-A, CEC-B pins if unused can be left unconnected.

  • In reply to Malik Barton57:

    Hello Malik-san,

    Thank you for your reply.

    I understand your comment.

    I will explain it to my customer.

    Best Regards,

    Y.Hasebe

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.