This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CD4066B: whether the CD4066B can support +-8v input signal

Part Number: CD4066B

Hi team,

I want to check the whether the CD4066B can support +-8v input signal. Thanks.

±8V

  • The electrical characteristics are specified only up to VDD = 15 V (± 7.5 V). Section 6.3 guarantees that the device works with up to 18 V (± 9 V), but there are no guaranteed eletrical characteristics for that.

  • In reply to Clemens Ladisch:

    Hi Clemens,

    So the conclusion is the device can be used for +-8v input, right?

    BR

    Frank

  • In reply to Frank Xiao:

    Yes, it can support ± 8 V inputs.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.