This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TINA/Spice/CD4053B: CD4053B SPICE model

Intellectual 990 points

Replies: 6

Views: 922

Part Number: CD4053B

Tool/software: TINA-TI or Spice Models

Is there a SPICE model available for CD4053B?

If not, how can I approximate via inputs to a user-generated model?

Thanks.

Greg

  • Greg, we don't have a spice model for the CD4053B. What parameters are you interested in evaluating using the model? A simplified user model would be to simply implement a series resistor & loading capactiance based on the datasheet values.

    -Ravi
    Systems & Applications Manager
    MUX & Signal Switches

     

  • In reply to Ravi Singh:

    Ravi,

    How would one model cross talk between channels? Thanks.

    Greg
  • In reply to Gregory Duperon:

    Greg, crosstalk can be tricky to model using a simplified switch model. Fundamentally, it is parasitic coupling between adjacent channels, however it is best modeled using silicon data characteristics.

    The CD4053 datasheet has freq/crosstalk listed for -40dB level. Is there a specific frequency range & configuration you need? Can you share some background on what is driving the crosstalk modeling request?

    -Ravi
    Systems & Applications Manager
    MUX & Signal Switches

     

  • In reply to Ravi Singh:

    test
  • In reply to Braon Moseley:

    Hi Braon,
    Sorry about the delayed response. I was out of the office when your e2e post came in.

    We have ordered a couple of CD4053 units to generate a typical cross-talk plot in the lab. Should be ble to follow up by end of week with an update.

    -Ravi
    Systems & Applications Manager
    MUX & Signal Switches

     

  • In reply to Ravi Singh:

    Hi Baron,

    With below pin out of CD4053B:

    To measure Ax OR Ay to Ay cross talk (pin 14 to pin 13, switch closed on ax), the channel input and output is connected to the network analyzer as below.

    The equation used to generate the plot is:

    Crosstalk (dB)= 20log(Vout/Vs)

    Where
    VS : Voltage applied to source pin of on channel
    VOUT: Voltage measured at output pin of off channel

    A general cross talk graph is represented as frequency (Hz) vs magnitude (dB)

     

    Similarly, below graph is the Bx OR By to By( pin 15 to pin 1, Bx switch closed): 

    Similarly, below graph is the Cx OR Cy to Cy( pin 4 to pin 3, Cx switch closed):

    Please let me know if you have any further questions.

    Thank you.

    Regards,

    Helen

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.