This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TS3A227E: INT pin connection when manual I2C control is enabled

Prodigy 20 points

Replies: 1

Views: 229

Part Number: TS3A227E

Hello,

Datasheet of the part states that INT pin must be grounded when I2C is not used. Can this pin be tied to ground when manual I2C control is used, but INT pin is not needed?

What I could find from the forum:

"The INT/ and MIC_PRESENT/ pins are status indication pins for communication back to the system. These are to let the system know that there are changes in the TS3A227E. If your system doesn't need to know something changed with the TS3A227E (int pin) or has detected a microphone (MIC present pin) then you may ground the pins

...

Thank you,
Adam"

Br,

Kasperi

  • Kasperi,

    The INT/ pin is simply an open drain output.  You may connect this pin to ground if it is not in use.  

    Thank you,

    Adam

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.