This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TS3L501E: Can TS3L501E being put after the transformer of the connector?

Intellectual 1465 points

Replies: 2

Views: 177

Part Number: TS3L501E

Hi,

My customer is looking for LAN switch, but they want to put the controller after the transformer of the connector, which is the same side with the ethernet cable.

Please see below picture: 

May I ask if this configuration is available to use? 

Thanks for your help.

  • User021864,

     

    The TS3L501E is a  bidirectional passive FET switch so it doesn't matter where you put the switch in the system as long as the voltage and currents exposed to the device are within the recommended operating conditions.

    The most common issue people run into with using this device is exposing it to negative voltages which are outside the recommended operating conditions.

    Thank you,

    Adam

  • In reply to Adam Torma:

    Dear Adam,

    Thanks for your explanation.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.