This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

SN74CBT3125: When OE# signal assert, the Pin A and Pin B status

Prodigy 40 points

Replies: 3

Views: 321

Part Number: SN74CBT3125

Hi sir,

    I have two question need confirm about SN74CBT3125 as bellows:

(1) When  SN74CBT3125 OE# signal assert, the Pin A and Pin B status. Does the pin A and Pin B is unstable status or tri-state?

(2)  When  SN74CBT3125 OE# signal assert, the pinA have 3.25MHZ signal , does it have risk to damage the SN74CBT3125?

Thanks

yanan

  • Yanan, 

    1) When the OE pin is logic low there will be a low impedance path between A and B pins.  When OE pin is logic high there will be a high impedance path between pin A and Pin B. 

    2) The SN74CBT3125 may accept any signal from 0 to Vcc and less than <128mA if OE is logic high or logic low.

    Thank you, 

    Adam 

  • In reply to Adam Torma:

    Hi Adam,
    It seems there have some misunderstanding about the question 1.
    When the OE pin is logic high, there will be a high impedance path between pin A and Pin B. But what the status about the Pin A or Pin B? Is it tri-state or unstable status( sometimes high and sometimes low)?

    Thanks
    yanan
  • In reply to user5288154:

    Yanan,

    The SN74CBT3125 is a passive FET switch and doesn't have any buffering which I don't think it is 100% valid to use the term Tri-state which implies a buffered output. You will simply see Hi-Z looking into either A or B pin when the signal path is disabled.

    Thank you,
    Adam

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.