This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

Data sheet section 5 pin configuration and function mixed up

Genius 11605 points

Replies: 1

Views: 190

Part Number: sn74hc4066

Is there  an error in the datasheet for this part.

http://www.ti.com/lit/ds/symlink/sn74hc4066.pdf

 In section 5 Pin Configuration and Functions there are mixed up descriptions for the pins in the table (like 3 times Switch 1 for the inputs/outputs)  Thanks.

  • Naser,

    Thank you for bring up this to our attention.  The description should be corrected to match the switch number with the pin name number. 

    Thank you, 

    Adam 

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.