This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TS3A5223: TS3A5223 tpd specification

Mastermind 6825 points

Replies: 1

Views: 142

Part Number: TS3A5223

Hello

 

             Has TS3A5223 tps max specification due to just only tplh/tphl 0.2ns (typ) &1.8V specification on datasheet? Thank you.

 

BR

Patrick

  • Patrick,

    The propagation delay of the TS3A5223 is measured at different supply voltages.  Yes with Vcc = 1.8V the propogation delay is 200ps.  

    Why do you need to know the low propagation delay of this device?  

    Thank you, 

    Adam 

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.