This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TMUX1219: In the 2-to-1 mode, both directions are turned on at the same time. Is it feasible?

Expert 1640 points

Replies: 1

Views: 45

Part Number: TMUX1219

Hi 

In the 2-to-1 mode, both directions are turned on at the same time. Is it feasible?

Thanks

Elsa

  • Hi User,

    Are you asking if the device is a bi-direction mux?

    S1 and D will be connected at the same time.

    Are you asking if S1 and S2 can both be connected to the D pain? If so, this is not how the device works.

    Regards,

    Dakotah

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.