This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TS3DS10224: TS3DS10224 Datasheet Configuration Problem

Prodigy 20 points

Replies: 5

Views: 170

Part Number: TS3DS10224

Hi, while reading the TS3DS10224 datasheet, I found the following problem:

1. In Table 6 of the datasheet, there are 2 modes 0100 & 0101, see the capture below.

These two modes looks the same as 0000 & 0001 modes.

2. However, according to the logic block diagram, in both modes, the OUTB should be INB as well. Please find my illustration below.

Hence, would you please double check whether the description of these two configuration in Table 6 is wrong?

Thank you!

Best regards,

Yu An Wang

  • Hi Yu An,

    Can you upload the images again? Looks like they are not fully loaded.Or you can share them offline and I'll re-upload them here.

    Can you also try testing by switching the configuration and see if you get the same problem? Can you also share the block diagram of your application.

    Thanks

    Saminah

  • In reply to Saminah C:

    Hi Samina,

    I reattached the excerpts from datasheet below. Please check the 0100 & 0101 mode in the logic block diagram and the datasheet's Table 6.

    I have actually tested one sample of TS3DS10224 and it turned out the Table 6 is really incorrect.

    So I hope TI can revise the datasheet ASAP.

  • In reply to Yuan Wang1:

    Hi  Yu An,

    Thank you for your inputs. I am working on verifying the function table and updating the datasheet accordingly.

    I will let you know when the updated version is online.

    Thanks

    Saminah

  • In reply to Saminah C:

    Hi  Yu An,

    Just wanted to update you on this. I am still waiting for the board to test this device and then update the logic table.

    It may take end of next week to have the datasheet updated.

    Thanks

    Saminah

  • In reply to Saminah C:

    Hi  Yu An,

    I am still waiting on the board. I will re-open this thread and update once done with the testing.

    Thanks

    Saminah

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.