• TI Thinks Resolved

TMUX136: MUX recommendation for UART and CAN Bus?

Prodigy 400 points

Replies: 3

Views: 131

Part Number: TMUX136

Hi Team,

Is there MUX solution that can use for both UART and CAN Bus?

Thank you.

Tiffany Liu

  • Hi Tiffany,

    At the digital side, the TMUX136 can be used for both UART and CAN depending on the bandwidth requirements for your application.

    Can you provide an image of what you are trying to accomplish?  This way we can recommend the best device.

    Thanks

    Saminah

  • In reply to Saminah C:

    Hi Saminah,

    Sorry for late response. 

    Customer's spec changes to MUX for RS232 and CAN Bus (CAN Bus 2 sets). Bandwidth at 2Mbps.

    Thank you.

    Tiffany Liu

  • In reply to user4773196:

    Hi Tiffany,

    It depends on what is your RS232 and CAN voltage range. If it is within the recommended operating conditions of TMUX136 , you should be good.

    Bandwidth wise, I do not see any issue as TMUX136 has a high bandwidth (6Ghz).

    Thanks

    Saminah