• Resolved

TS5MP645: 1 :2 demux/switch

Prodigy 95 points

Replies: 2

Views: 76

Part Number: TS5MP645

We are planning to use TS5MP645 as 1:2 demux/switch, (Application: One camera is interfaced with two controllers according to the requirement). Is it feasible, since in datasheet the use case is 2:1 MUX/switch (and mostly applications are two cameras interfaced with a single controller). Please advise on the above.

Thanks 

Regards,

Muhammed Shajih