This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TS5A22364: May I know if TS5A22364 can support 3Vrms output for headphone? Peak voltage will be 4.3V? Hence, p2p voltage is 9V.

Mastermind 44210 points

Replies: 3

Views: 108

Part Number: TS5A22364

E2E, 

May I know if TS5A22364 can support 3Vrms output for headphone? Peak voltage will be 4.3V. Hence, p2p voltage is 9V. The output signal will pass through this TS5A22364 switch.

 

Thank you,

Adam

  • Hi Adam,

    TS5A22364 has a recommended signal path voltage range of 5.5V, so a peak-to-peak voltage of 9V is not recommended.

    Thank you for your interest, I will send your request to our product definition team to add to our creative backlog.

    Regards,

    Kate

  • In reply to Kate Dickson:

    Hi Kate,

    Since peak-to-peak voltage of 9V is not recommended, for the same application (headphone output) to use as click and pop noise reduction, can we TS5A22364 as shunt switch for mute where IN1 & IN2 are connected together as /MUTE as shown on the typical operating circuit below? NC1 is INL and NC2 is INR. 

    Thanks.

    Gim Song

  • In reply to Gim Song:

    Hi Gim Song,

    You may use TS5A22364 in this application, as long as your system operates within the recommended operating conditions in the datasheet.

    Regards,

    Kate

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.