• Resolved

CD74HCT4053: PN: CD74HCT4053 ESD HBM is ±500V? I don't think it's that low,Can you help confirm it. Thank you.

Intellectual 370 points

Replies: 4

Views: 86

Part Number: CD74HCT4053

Hi ;

    PN:  CD74HCT4053   ESD HBM is ±500V? I don't think it's that low,Can you help confirm it.  Thank you.

         

  • Hello,

    The datasheet shows that the actual rating for the ESD HBM is +/-500V.

    Are you looking for a device with a higher ESD HBM rating? I would be happy to recommend an alternative device.

    Regards,

    Kate

  • In reply to Kate Dickson:

    Hello Kate;

         The end Customer use CD74HCT4053 to test in progress。 but now find  ESD HBM is +/-500V;The customer thinks it should not be so low.

    Is there a mistake in the specification?  Is this IC ESD HBM that small?Which model do you recommend?  Can P2P completely replace CD74HCT4053? Thank you.

  • In reply to Tony xiong:

    Hello,

    I am checking on the ESD HBM specification for CD74HCT4053.

    TMUX1133 is a recommended pin-to-pin replacement for CD74HCT4053. The ESD HBM rating for TMUX1133 is +/-2000V. Please see the comparison of the two parts below:

    Best Regards,

    Kate

  • In reply to Kate Dickson:

    Hi Kate:

        Thank you.