This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3DDR4000 IBIS model/s-parameters

Other Parts Discussed in Thread: TS3DDR4000, TS3DDR3812

Is there an IBIS model available for the TS3DDR4000?

There is for the TS3DDR38112, but all recommendations are for using the new TS3DDR4000 instead of the "old" TS3DDR3812.

Thomas

  • Thomas,

    No, The TS3DDR4000 does not have an Input/output Buffer Information Specification (IBIS) model.  The TS3DDR4000 is an unbuffered pass FET so we recently decided it did not make sense to create a buffer information model since the signal path is not buffered.  However, we do have s-parameter models you can find in this E2E post  below.

    An ideal model of the signal path will be a 0 ohm short but in practice there is a series resistance (Ron) and an input capacitance (Con) to ground on the signal path.  These parasitics are provided in the electrical specifications in the datasheet.

    Thank you,

    Adam

  • Hi Adam,

    Thank you very much for the link to the S-parameters.

    I see what you mean, I just asked because IBIS models are available for other analogue switches. I'll see if I can figure out how to use the S-parameters instead, it should be possible.

    Thomas