This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS5A23157: Current source of output

Part Number: TS5A23157

Hi Team,

When load resistance connect to TS5A23157 and input 5V to TS5A23157, what is source of output current?
Output current source from input 5V or supply or TS5A23157 internal block?
Thank you.

Best Ragards,
Jade

  • Jade,

    The TS5A23157 is a passive FET switch.  The current passing through the switch will be calculated based on the source voltage and the load.  If you have 5V on the input of TS5A23157 and a 1k ohm load you would have 5 mA of current passing through the switch if your voltage source can drive the 1k load. 

    Let us know if that answered your question. .

    Adam