This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS5A26542: Extending the Input Logic Translation Vio range

Expert 6310 points
Part Number: TS5A26542
Other Parts Discussed in Thread: TMUX136

Dear Team,

TS5A26542 has a great feature of Input Logic Translation. The Vio range is only specified from 1.65 to 1.95V - Is this range extendable?

Thanks and regards

  • Bartosz,

    The TS5A26542 device absolute maximum spec for Vio is the same as V+ which tells me they use the same size transistors in the design. 

    You could connect V+ to Vio and have the digital logic thresholds Vih and Vil will scale according to the datasheet below.   

    What were the key specs you chose the TS5A26542?  If you are not using the logic translation feature would you consider a lower cost switch? 

     


     

     

    You can also look at the new TMUX136 which will support 1.8V logic.

     

    Thank you,

    Adam