Other Parts Discussed in Thread: TMUX136, TS5A23160, TS5A23159, TMUX1511, TMUX1072
Hi Team,
Our customer is considering to use TS3A5223 to switch I2C bus to select one of the two I2C master.
Q1). Can TS3A5223 be used to switch I2C Bus ? I believe there is no problem.
Q2). Since the absolute maximum rating is 4.3V, I believe the device would not get damaged even 3.3V applied to the NC/NO/COM pin when device not powered up. Am I correct ?
One of the I2C master uses separate power suppy (bus pull up voltage) and there is a case where bus pull up is enabled and TS3A5223 is powered down.
Q3). What is the reason that the maximum recommended VNC/VNO/VCOM is limited to "VCC" ?
Best Regards,
Kawai