This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 142
Part Number: TS3A5223
Hello
Has TS3A5223 tps max specification due to just only tplh/tphl 0.2ns (typ) &1.8V specification on datasheet? Thank you.
BR
Patrick
Patrick,
The propagation delay of the TS3A5223 is measured at different supply voltages. Yes with Vcc = 1.8V the propogation delay is 200ps.
Why do you need to know the low propagation delay of this device?
Thank you,
Adam