hi dear supporting team,
understand that before powering up SN74CB3Q16244 I/O will be hi-z status. so that means even if customer apply -0.5~7V which is absolute rating range at switch I/O when Vcc=0V, is it ok without damage the chip? and after power up, the chip could still work normal if the I/O voltage goes to recommend condition? tks a lot!