Other Parts Discussed in Thread: TMUX1209
Hi all,
There is something confusing about CD4052 application.
And according to the datasheet of CD4052, the min of input high voltage is 3.5 V under VDD=5v condition, but 3.3V coming from MCU also can pass the test!
I doubt whether is there any risk on this application or need I do the level *** to satisfy the voltage request?
looking forward to your reply!
BR!