This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TS3USB30: Can device be powered from VBUS at 5V. ?

Mastermind 44330 points

Replies: 1

Views: 79

Part Number: TS3USB30

e2e, 

I would like to know whether it can be powered from VBUS at 5V. the datasheet spec for Vcc runs upto 4.3V so I’m inclined to say that is not supported. The max rating does go up to 7V but I think that’s not for extended periods of operation, right?

Thank you,

Adam

  • yes, only upto 4.3v. TS5USBC401 can handle Vcc upto 5.5v.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.