This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CBT3125: Power the switch chip from an I/O pin output

Part Number: SN74CBT3125

Can we connect the VCC pin of this SN74CBT3125 switch chip to an I/O pin of a 430 MCU? In other words, can we use the I/O pin output of a 430 MCU  to supply the power to the switch chip? What we want to do is to control the power supply of the switch chip using a 430 MCU.  We are not sure:  1. How much current will the switch chip draw from its VCC pin when its VCC voltage is about 2.8-3.0V.   2. Whether the SN74CBT3125 switch can work properly under 2.8V VCC.  The datasheet says  the recommended power supply is 4V.  2.8V is quite far from 4V.  3. What is the output current of the I/O pin of a 430 MCU, assuming the 430 MCU is powered by a 3V power supply?  Thanks a lot for the help.