This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CBTD1G125: looking for switch solution with level shifting function

Part Number: SN74CBTD1G125
Other Parts Discussed in Thread: TXS0102, LSF0102, SN74AVC2T245

Dear expert,

Did we have 2 channel switch with level shifting function integrated for UART interface?

The voltage of input UART is 3.3~5V, but only 1.8V acceptable at out put side.

Thanks.

Regards,

Ben