Other Parts Discussed in Thread: TS3A5223
I am using SN74LVC1G3157 with Vcc = 3.3V
Page 3 of the datasheet recommends that the maximum of dt/dv = 10ns/V
However, I2C signal's falling time could be as long as 300ns, far exceeding the recommended maximum of dt/dv =10ns/V. The input signal slew rates matter for clocked flip flops or latches.
My questions are:
(1) Is "the maximum of dt/dv =10ns/V" a hard requirement?
(2) What happens if my inputs do not meet this requirement of " the maximum of dt/dv =10ns/V"?
Thanks