Other Parts Discussed in Thread: MPC508
Hello guys,
One of my customers was about to use MUX508 for their new products.
But they stopped to use the MUX because they need MUX which can be applied about 15V to input when the MUX is powered off?
MUX508 input absolute maximum is VSS-2V ~ VDD+2V.
Do you have any MUX product has VSS-10V ~ VDD+10V as input absolute maximum rating?
Your reply would be much appreciated.
Best regards,
Kazuya.