• TI Thinks Resolved

TS12A4514: switch state if Power-off

Expert 2320 points

Replies: 1

Views: 44

Part Number: TS12A4514

Hello

What is the switch state if the power is off?

(ON, OFF, High-Z)

Is the device connected to a specific port when the power is turned off?

Best regards

  • Hi Louis,

    The TS12A451x parts have protection diodes to Vcc, So you must not apply voltages to COM/NO/NC when powered off.

    The Off leakage specs in the datasheet provide the current information (Vcc = 0V):

    regards

    Saminah