This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2G66: About ICC value at VCC=1.9V, 3.8V, 5.0V and TA=-10℃ to 40℃

Guru 21045 points
Part Number: SN74LVC2G66

Hi Team,

 

We understand that ICC is 10uA(max) at VCC=5.5V, TA=-40℃ to 85℃ and ICC is 1uA(max) at VCC=5.5V, TA=25℃.

However, we would like to know about ICC value at VCC=1.9V, 3.8V, 5.0V and TA=-10℃ to 40℃.

Could you please let us know if you have a “VCC vs ICC vs TA Graph”?

 

Regards,

Hide