• Resolved

TS3V340: S2 voltage when D connect to S1

Part Number: TS3V340

Hi Sir,

When we set D(0V) connect to S1 and S2 is floating, we could measure a 0.3C~1V on S2 pin.

Could you help to explain why S2 is not 0V?

Many thanks,

Patrick 

  • Hi Patrick,

    As shown in this App Note  floating pins can have all sorts of implications. 
    What is the VCC level and are all other signals disconnected? If not, what are their signal levels and frequencies?

    Thank you and best regards,

    Ambroise

  • In reply to Ambroise Suter:

    Hi Ambroise,

    D: LVDS signal.

    S1: DC level = 0V with external DC cap blocking.

    S2: floating.

    Many thanks,

    Patrick 

  • In reply to Patrick Chen(TPE System & Application):

    Hi Patrick,

    depending on the frequency and voltage level the LVDS signal is running at, it could contribute up to 0.26V (500MHz, 3.3V) due to off-isolation (Figure 3 in the Datasheet).
    Other sources could come from parasitics within the CMOS switch.

    Best regards,

    Ambroise