Hello,
I will use on new electronic board (see attached schematic).
The headphones will be driven by a single ended audio amplifier (the output voltage will be in range 0-5V).
C1, C2 are DC blocking capacitors, they are used to suppress offset voltage, so the TIP signal will be in range -2.5V/+2.5V.
But, when C2 ( or C1) is not charged, it's acts as a short circuit, and if the output voltage of the amplifier is at 5V, the signal "TIP" will be also at 5V.
The datasheet specifies a maximum level on TIP signal of VDD+0.5V = 3.3+0.5 = 3.8V.So the TIP signal will therefore be out of specification during few ms.
May it be a problem?
Do you have a proposal to avoid this?
Thanks.
Best Regards.
Sylvain