E2E,
I'm trying to use a low capacitance switch to switch two inputs that are connected to the feedback to switcher’s FB node (one for local sensing and the other for remote sensing).
I need to make sure that one of the inputs make it to the output since it is required to be present always even during the switches transition. I need to make sure their voltages levels are likely on the same ball park during the transition, and we need to ensure that FB pin is biased by one of the inputs.
I didn't see many make before break options for switchs but I found this technote that shows a similar use case with a mux in the feedback loop using a 1:1 SPST.
Improve Stability Issues with Low CON Multiplexers
Is this a better solution?
Thank you,
Adam