This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

SN74HC4851-Q1: Smallest leakage current in ON-state

Guru 11255 points

Part Number: SN74HC4851-Q1

Hi

We are looking for 8:1 analog multiplexer which has the smallest leakage currennt with ON state in automotive grade (Q1)
The following is our requirement.

・8 : 1 analog MUX/DEMUX
・Smallest leakage in ON-state
・Automotive grade
・Temperature range -40℃ to 85℃

For example, maximum IS(on) is +/-0.5uA in -40℃ to 85℃ in SN74HC4851-Q1 but those of SN74LV4051A-Q1 is +/-1uA in -40℃ to 105℃.

It seems that IS(on) of SN74HC4851-Q1 is better than that of SN47LV4051A-Q1 but we can't see the thing of fact because the temperature range is different.

Which device can offer the smallest on-state leakage?
Or do you have any other device which has small leakage current?

BestRegards

  • Hi Na na,

    Both the SN74HC4851_q1 and the SN74LV4051-Q1 are the lowest IS(on) automotive quality switches we have. 

    The SN74HC4851-Q1 calls out a lower specs as you mention (+/-0.5uA) at 85C while the other device does not specify at the 85C temperature. I would agree with you and choose the SN74HC4851-Q1 since the datasheet calls out a lower spec. 

    Regards,

    Dakotah

  • Guru 11255 points

    In reply to Dakotah:

    Hi Dakotah

    Thank you for your reply.

    I understood.

    BestRegards

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.