This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TS5A23159: Which 2:1 switch can be used for DP AUX?

Part Number: TS5A23159

Hi Team,

My customer is looking for 2:1 switch for DP AUX pins. They are requesting 3.3V power supply and low power consumption(they only need for DP AUX pins so High speed line is not necessary at this time). Do you have any recommended devices such the use case?

I'm wondering if we can recommend the following devices.

TS5A23159
TS3A44159

Any recommendation will be highly appreciated.

Regards,

Takashi Onawa

  • Hello Onawa-san,

    I have looked into the DP AUX standard (Page 34):

    and if they are using the default speed of 1 Mbps, then either switches will work for their applications. However, if they wish to use the fast mode, also on page 34, then they will need a switch with a much higher bandwidth. 

    Could you tell us which data rate they will be operating the DP AUX at?

    Thanks,

    Louie

  • In reply to Louie:

    Hi Louie-san,

    Thanks for your prompt response on this.
    They don’t use fast mode. so the data rate should be 1Mbps.

    Regards,
    Takashi Onawa
  • In reply to Takashi Onawa:

    Hello Onawa-san,

    That's perfect, our switches should be more than capable of handling that speed.

    Thank you,
    Louie

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.