SN74LVC1G3157: What is the maximum current through this device

Part Number: SN74LVC1G3157

HI,

I am developing an application in which I need to switch between a gate driver output and a resistor. 

lets say 

when S=1 

A = gate driver output

When S=2

A= Connected to resistor

I need to know can SN74LVC1G3157 handle the output current of the gate driver?

What is the maximum current that can flow through this device from B1/B2 to A?