• TI Thinks Resolved

CD4051B: MUX/DEMUX LIN bus

Part Number: CD4051B

Hello,

I would like to multiplex 5 LIN slave to my master (those slaves can't be on the same LIN bus).

I selected a TI transceiver from UART : TL2029.

I think that a CD4051B could work because Vdd can be up to 20V (that would eliminate a sn74cbt3251).

Is there any EVM available with this chip and/or would recommend another chip ?

Thanks