Hello,
i am designing a Hardware in which i am switching a precise current source of value 0.09 milli ampere using cd4051 multiplexer.
my circuit contains two stages 1st D-MUX stage and 2nd MUX stage. as explained in below picture.,
i tested this circuit using cd 4051 DIP package. If i switch current through 100k (0.1%) resistor i get output 9 volt.
the problem is when i replace the DIP package with smd package, for 100 k it gives 7.6 volt and reduces to 6 volt
then i cross checked using dip package in same circuit it give perfect result.
CAN ANY ONE PLEASE EXPLAIN???????????????