This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3DV642: May we have Displayport 1.2 switch with re-driver IC? or can we use TS3DV642 + redirver IC?

Part Number: TS3DV642
Other Parts Discussed in Thread: HD3SS212, HD3SS213, HD3SS215, HD3SS214, SN75DP130

Hi Sir

May we have Displayport 1.2 switch with re-driver IC? or can we use TS3DV64 + redirver IC?

if yes, may you have suggest ic?

                                                  Bogey

  • Bogey,

    The TS3DV642 is a passive FET switch, which can be ideally modeled as a 0 ohm wire, so it will not be an issue to use with a redriver. I will move this thread to the consumer and computing forum for assistance with a redriver.

    Thank you,
    Adam
  • Hi Chen,

    The TS3DV642 doesn't belong to our group, we have the passive switches HD3SS212, HD3SS213, HD3SS214 and HD3SS215 depending on your needs.
    For DP1.2 you can use SN75DP130 as a redriver and SNx5DP159(x-mode) as retimer.
    Since we don't have switches with EQ for DP, you will need a two chip solution.

    Regards