This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS12A12511: Analog switch to pass signal with -8 to 8 V at 500 kHz

Part Number: TS12A12511
Other Parts Discussed in Thread: CD4066B, CD4016B, MUX509

Hi, I'm looking for an analog switch to pass a voltage signal from a function generator with characteristics -8V to 8V at 500 kHz.  The specifications of the TS12A12511 besides the 6 Vpp limit are fine for my application. I also found the switch CD4066B but it's limited to 7.5 Vpp.  Can you provide a list of products that will satisfy these basic requirements? 

Thank you. 

  • Melida,

    I'm sorry it is not easy to search this basic requirement on TI.com. We will have an easy way for you to conduct you search of simple switch parameters in April 2017.

    In the mean time here are some devices I could find for you that could pass -8 to 8 V signals.

    CD4016B
    MUX509
    MPC509A

    Thank you,
    Adam