Other Parts Discussed in Thread: TS3A24159
Hello support team,
Our customers is evaluating TS3A5223 now.
In the customer's circuit as shown in the figure, 1.8 V is supplied to Vcc, and the voltage generated from 3.3 V is applied to COM1 at Vcc = 1.8 V.
When SEL1 is 'H', voltage at NO1 is as expected at 1.65V.
When SEL 1 is 'L', voltage at NO1 should be 0 V, but it is around 1.15 V.
It seems that the switch does not turn off and leaks.
In the data sheet, the upper limit voltage of the input terminals NOx and COMx is not limited by Vcc.
However, I think that these input voltages have no tolerance above Vcc.
Is my understanding wrong?
Best regards,
M. Tachibana