This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3A27518E-Q1: Regarding IBIS model for TS3A27518E-Q1

Part Number: TS3A27518E-Q1

Hi

While performing the Hyperlynx simulation using IBIS model i could not find the connectivity once i import the IBIS model.

Can you please provide me the correct IBIS model for the same.

I have attached the same for your reference.

Regards

Nitesh

  • Hi Nitesh,

    Can you clarify what are you trying to accomplish with the Input/output Buffer Information Specification (IBIS) model? ? This device is only a pass FET and therefore an IBIS model may not provide you with much useful information. Please see attached E2E post on why this may not be suitable for your simulation needs. 

  • Hi Dakotah

    Thanks for the reply.
    Since i have used the same part in the design so we need to simulate as per the board file generated where we have to load the IBIS model for the IC's.
    So we need the Model for simulation.

    Regards
    Nitesh
  • Hi Nitesh,

    To clarify my last post. IBIS models are typically used for devices with buffered inputs and outputs. The only buffered inputs we have are our select and enable pins. The actual signal path is not buffered so they typically do not make IBIS models for these switches.

    Do you still need an IBIS model or is it not needed?

    If you do need an IBIS model, we will need to know which parameters are most critical for the modeling team. If they can create a model please allow at least 2-4weeks for the team to create it.
  • Hi Dakotah

    Thanks for the reply.

    I need to check on signal information .

    Regards

    Nitesh