Dear e2e community,
When when my customer connects a usb cable, the ADC value indicates "11111". The switch seems to be in open state at that time.
As there are 4 possible Switch States, for this ADC value, which one should we consider at the initialization?
In ohter worlds, what is the default switch state (USB/UART or OPEN?) when ADC indicates "11111"?
Device Type 1 and Device Type 2 registers = 0x00
Regards,