Hi Team,
Please help to confirm the Pd(W) and Thjc(C/W) of TS3V713EL
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Daniel,
TS3V713EL has two supplies, VDD and VDD_5. The current drawn from these two supplies are IDD (max) = 500uA and IDD_5 (max) = 50uA.
When VDD = 3.6V and VDD_5 = 5.5V, the maximum power disspation is
3.6V * 500uA + 5.5V * 50uA = 2.075mW.
You will also need to consider the power going through the switch which will be W=(Ii/o)(Ron^2) for each channel
Our package thermal resistance shows as 39.2 Degree C per Watts.
You can see more information on this posting which includes a calculator