Other Parts Discussed in Thread: TS12A44515, SN74HC4066
Hey Team,
I was hoping you could help me with a quick question.
So I am looking at our: TS12A4451x device and comparing it to the competitor: 74LVC4066PW
And the cross reference tool suggests the TS12A44513 which has 2 NC and 2 NO paths, but the other device seems to have 4 NO (normally Open, or “Off”) paths. This is just one of the differences, but seems to be the major one. I wanted to get your thoughts on if the TS12A44515 might be a better fit or another device all together.
In general could you take a look at that other device and ours and see if there are any other major differences? The other item I saw was that our device has a much larger input voltage range:
2V -> 12V (Ti) vs. 1.65V-> 6.5V (Nexperia)
-0.2V -> 13V (abs max TI)
Let me know if you can help clarify this. Thanks!
Best Regards,
Saqib Mohammad