Dear expert,
I'm using the TS3A24159 as a switch between 2 Uart devices. I'm seeing about a 2% failure with these devices in production and cannot seem to pinpoint the problem. When both devices are connected (via external cable), only the NO device communicates with the host processor. If I only connect the NC device, it works fine and same if both or only the NO device is connected. Please see schematic below and let me know if you see anything I can check that could potentially cause this problem.
When verifying the signals with an oscilloscope, the device that is not working never sees the TX from the host indicating that the switch isn't closed or somehow between states.
Operating parameters:
9600 BAUD
1mS delay between communications and switching
End devices are 2 of the same microcontrollers.
Regards,
Dan Hughes