This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3A44159: For high voltage ultrasonic switching

Part Number: TS3A44159
Other Parts Discussed in Thread: TMUX6104

Hello,

I am using the TDC1000-7200 GASEVM for liquid ultrasonic sensing using 1MHz transducers and I need a 2:1 switch for impedance matching the Tx and Rx lines. I managed to use the TS3A44159 without the boost converter as it can handle 5V and it worked fine. Now I need to find a similar switch in terms of T_off/on time and channels that can handle up to 30V input signals that the boost converter provides. 

I tried to ask in the ultrasonic sensing forum but I have not gotten any answer. 

Do you have any suggestion of suitable switch from you or third party? 

Thanks

Regards
Thibault