This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CB3T3257: Whether there is another part to support output voltage translation tracks VCC which is up to 5V in typical?

Part Number: SN74CB3T3257
Other Parts Discussed in Thread: TS3A5018, CD40109B

I would like to find a 4-BIT 1-OF-2 FET MULT/DEMUL, like as SN74CB3T3257, to support output voltage translation tracks VCC and the VCC can up to 5.5V or more. Customer hop to have 3.3V input and 5V output with this Mux.