Hi,
I see leakage current specs for IN pin in datasheet. Does it mean the current required to drive the IN pin too?
Thanks.
- YY
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I see leakage current specs for IN pin in datasheet. Does it mean the current required to drive the IN pin too?
Thanks.
- YY
YY,
The TS5A3166 IN pin is the digital control logic pin which determines weather or not the signal path is conducting (low impedance) or Hi-Z.
This IN pin is basically connected to an inverter inside the IC.
The digital control input leakage spec states that if the IN pin is supplied with 5.5V or 0V <+/-20nA of current will flow in or out of the pin. Another way you can interpret this spec is that is it is a high impedance buffer and you won't necessarily need a strong driver to toggle the pin.
Thank you,
Adam